AXIS#.STOP

Description

This command stops drive motion. In torque and velocity modes, the command value will immediately be set to 0. In position mode, the axis will decelerate to a full stop. If the position command is from a gearing master, the drive will cancel gearing and decelerate to a stop. This command has no effect if the command source is an analog input.

If the command values are coming from a fieldbus master, the stop may be immediately overwritten by a new fieldbus command. Use a controlled stop input or disable command to ensure a stop.

The following table defines the behavior of AXIS#.STOP:

Cmdsource Opmode Subopmode Deceleration ramp defined by:
Service Torque - AXIS#.IL.CMD = 0
Velocity - AXIS#.SM.DEC and AXIS#.SM.DEC 
Position Service motion AXIS#.SM.DEC and AXIS#.SM.DEC 
Motion tasking AXIS#.MT.DEC
Homing AXIS#.HOME.DEC
Fieldbus Torque - Command has no effect.
Velocity
Position
Electronic Gearing Position - AXIS#.GEAR.DECMAX
Analog Torque - Command has no effect.
Velocity
Position

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Command

Units

N/A

Range

N/A

Default Value

N/A

(missing or bad snippet)

N/A

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported

Industrial Ethernet Information

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5016

1

5016 (0x1398)

AXIS1.STOP

Unsigned8

Read/Write

No

70552

2

5016 (0x1398)

AXIS2.STOP

Unsigned8

Read/Write

No

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.STOP

5016

Unsigned8

Read/Write

-